| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Sub ApplyChanges() | |
| C# | |
|---|---|
public abstract void ApplyChanges() | |
| C++/CLI | |
|---|---|
public: abstract void ApplyChanges(); | |
If IsImmediateChangesEnabled is true, changes are processed immediately, and this method will have no affect. Processing changes has the affect of causing the data consuming Measurement to be preset to a default state. It will also cause any data in the internal buffers to be cleared.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)