Keysight 89600 VSA .NET API
SetFrequencyParameters(Boolean,Double,Double) Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > UserInputSetup Class > SetFrequencyParameters Method : SetFrequencyParameters(Boolean,Double,Double) Method


isComplexData
Specifies if complex data will be provided by data source application (sometimes referred to as Zoom mode when center frequency is specified as non-zero.)
centerFrequency
Specifies center frequency the data consuming Measurement should assume for data provided by data source application.
sampleRate
Specifies sample rate the data consuming Measurement should assume for data provided by data source application.

Glossary Item Box

Sets frequency parameters.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Sub SetFrequencyParameters( _
   ByVal isComplexData As Boolean, _
   ByVal centerFrequency As Double, _
   ByVal sampleRate As Double _
) 
C# 
public abstract void SetFrequencyParameters( 
   bool isComplexData,
   double centerFrequency,
   double sampleRate
)
C++/CLI 
public:
abstract void SetFrequencyParameters( 
   bool isComplexData,
   double centerFrequency,
   double sampleRate
) 

Parameters

isComplexData
Specifies if complex data will be provided by data source application (sometimes referred to as Zoom mode when center frequency is specified as non-zero.)
centerFrequency
Specifies center frequency the data consuming Measurement should assume for data provided by data source application.
sampleRate
Specifies sample rate the data consuming Measurement should assume for data provided by data source application.

Remarks

Using this method is equivalent to setting the IsComplexData, CenterFrequency, and SampleRate properties simultaneously. This sets properties for all channels. Use Channels to get or set properties of individual channels.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also