Gets the list of available
EventCondition types that can be used. Use the
Keysight.SA.Vsa.EventRule.SetExtension``1 method to select which
EventCondition is used. Obsolete. Use
GetAvailableExtensionTypes instead.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Function GetAvailableConditionTypes() As Type() |
| C# | |
|---|
public abstract Type[] GetAvailableConditionTypes() |
| C++/CLI | |
|---|
public:
abstract array<Type^>^ GetAvailableConditionTypes(); |
Return Value
array of
EventCondition types
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also