Keysight 89600 VSA .NET API
DownlinkUser Class
Members  See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : DownlinkUser Class


Glossary Item Box

The Lte.DownlinkUser class contains properties and methods specific to LTE Downlink users.

Object Model

DownlinkUser ClassAllocationCollection ClassAllocation ClassAllocation ClassLayerCollection ClassLayer ClassLayer Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class DownlinkUser 
   Inherits Channel
   Implements Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3 
C# 
public abstract class DownlinkUser : Channel, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  
C++/CLI 
public ref class DownlinkUser abstract : public Channel, Agilent.SA.Vsa.IPropertyInfo, Agilent.SA.Vsa.IPropertyInfo2, Agilent.SA.Vsa.IRemoteNotifyPropertyChanged, Agilent.SA.Vsa.IRemoteNotifyPropertyInfoChanged, Agilent.SA.VsaInternal.IObjectModel, Agilent.SA.VsaInternal.IObjectModel2, Agilent.SA.VsaInternal.IObjectModel3  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also