Keysight 89600 VSA .NET API
DownlinkUser Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace : DownlinkUser Class

Glossary Item Box

The following tables list the members exposed by DownlinkUser.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyActiveGets or sets a value indicating whether the channel is present in the signal. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyAllocationsGets the AllocationCollection associated with this channel. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyCodebookIndexGets or sets the Codebook Index for the DL user.  —
Public PropertyCW1McsIndexGets or sets the CW1 MCS index for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)20.0
Public PropertyCW1ModTypeGets or sets the modulation type for Code word 1 of the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyCW1PowerBoostGets or sets the per-subcarrier power boost in dB of Code word 1 of the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyCyclicDelayDiversityGets or sets the Cyclic Delay Diversity for the DL user.  14.00
Public PropertyCyclicShiftGets or sets the Cyclic Shift for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyDmrsCyclicShiftGets or sets the DRMS Alpha for the allocation/channel (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyDmrsGroupGets or sets the DRMS Group (u) of the allocation/channel (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyDmrsPowerBoostGets or sets the per-subcarrier DMRS power boost in dB for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyDmrsSeqGets or sets the DMRS sequence (v) for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyFormatGets or sets the PUCCH format for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyFrameIndexGets or sets the frame index for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyIncludeGets or sets a value indicating whether the channel is included in EVM calculations and shown in traces. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsAutoSyncEnabledGets or sets a value indicating whether synchronization slot is selected automatically. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsCW0EnabledGets or sets a value indicating whether or not CW0 is allocated to the DL user  —
Public PropertyIsCW1EnabledGets or sets a value indicating whether or not CW1 is allocated to the DL user  —
Public PropertyIsCW1McsIndexCoupledGets or sets a value indicating whether the all the allocations of the DL user share the same CW1 MCS Index.  20.00
Public PropertyIsCW1ModTypeCoupledGets or sets a value indicating whether the all the allocations of the DL user share the same CW1 Mod Type.  —
Public PropertyIsCW1PowerBoostCoupledGets or sets a value indicating whether all the allocations of the DL user share the same CW1 Power Boost.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsDmrsPowerBoostCoupledGets or sets a value indicating whether all the allocations share the same DMRS Power Boost. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsFrameIndexCoupledGets or sets a value indicating whether all the allocations of the DL user share the same Frame Index.  —
Public PropertyIsMcsIndexCoupledGets or sets a value indicating whether all the allocations share the same MCS index. (Inherited from Agilent.SA.Vsa.Lte.Channel)20.00
Public PropertyIsMirroringEnabledGets or sets a value indicating whether mirroring is used (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyIsModTypeCoupledGets or sets a value indicating whether all the allocations share the same mod type. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsPerAntennaEpreCoupledGets or sets a value indicating whether all the allocations share the same Per-antenna EPRE value  15.00
Public PropertyIsPowerBoostCoupledGets or sets a value indicating whether all the allocations share the same Power Boost. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsRBEndCoupledGets or sets a value indicating whether all the allocations share the same RB End. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsRBStartCoupledGets or sets a value indicating whether all the allocations share the same RB Start. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyIsUersActiveGets or sets a value indicating whether UE-specific RS is present for the DL user  —
Public PropertyIsUersIncludedGets or sets a value indicating whether UE-specific RS of the DL user is included in EVM calculations and shown in traces.  —
Public PropertyLayersGets the LayerCollection associated with the DL user.  —
Public PropertyMcsIndexGets or sets the MCS index for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)20.0
Public PropertyModTypeGets or sets the modulation type for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyNameGets or sets the name of the allocation. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyNPucch1Gets or sets n^(1)_PUCCH used to determine PUCCH cyclic shift for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyNPucch3Gets or sets n^(3)_PUCCH used to determine PUCCH cyclic shift for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyNumberOfCodewordsGets or sets the Number of Code words for the DL user.  —
Public PropertyNumberOfLayersGets or sets the Number of Layers for the DL user.  —
Public PropertyOSGets or sets the Orthogonal Sequence for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyPerAntennaEpreGets or sets the per-antenna EPRE in dB of the allocation/user. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)15.00
Public PropertyPowerBoostGets or sets the per-subcarrier power boost in dB for the allocation/channel. (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyPrecodingGets or sets the Precoding format for the DL user.  —
Public PropertyRBEndGets or sets the RB end for the allocation/channel (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyRBStartGets or sets the RB start for the allocation/channel (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertyRntiGets or sets RNTI for the user  —
Public PropertySlotEndGets or sets the Slot end for the allocation (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertySlotStartGets or sets the Slot Start for the allocation (Inherited from Agilent.SA.Vsa.Lte.AllocationBase)—
Public PropertySyncSlotGets or sets the slot to sync on. (Inherited from Agilent.SA.Vsa.Lte.Channel)—
Public PropertyUersNScramblingIdGets or sets the n_SCID for the generation of UE-specific RS for the DL user.  —
Public PropertyUersPowerBoostGets or sets the per-subcarrier Power Boost in dB of UE-specific RS of the DL user.  —
Public PropertyUersTransmitterPortNumberGets or sets the antenna port that UE-specific RS is transmitted on for the DL user.  14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also