Keysight 89600 VSA .NET API
IsFrameIndexCoupled Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > DownlinkUser Class : IsFrameIndexCoupled Property


Glossary Item Box

Gets or sets a value indicating whether all the allocations of the DL user share the same Frame Index.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsFrameIndexCoupled As Boolean
C# 
public abstract bool IsFrameIndexCoupled {get; set;}
C++/CLI 
public:
abstract property bool IsFrameIndexCoupled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also