Keysight 89600 VSA .NET API
Precoding Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > DownlinkUser Class : Precoding Property


Glossary Item Box

Gets or sets the Precoding format for the DL user.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Precoding As SharedChannelDecoderType
C# 
public abstract SharedChannelDecoderType Precoding {get; set;}
C++/CLI 
public:
abstract property SharedChannelDecoderType Precoding {
   SharedChannelDecoderType get();
   void set (    SharedChannelDecoderType value);
}

Property Value

The default value is SharedChannelDecoderType.Off.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also