Keysight 89600 VSA .NET API
UersPowerBoost Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > DownlinkUser Class : UersPowerBoost Property


Glossary Item Box

Gets or sets the per-subcarrier Power Boost in dB of UE-specific RS of the DL user.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property UersPowerBoost As Double
C# 
public abstract double UersPowerBoost {get; set;}
C++/CLI 
public:
abstract property double UersPowerBoost {
   double get();
   void set (    double value);
}

Property Value

The default value is 0 dB.

Remarks

This property is valid only in TDD mode.

This property is valid only if IsUersActive is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also