Keysight 89600 VSA .NET API
AntennaArrayShape Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : AntennaArrayShape Property


Glossary Item Box

Gets or sets the Antenna Array Shape.

Syntax

Visual Basic (Declaration) 
Public Overridable Property AntennaArrayShape As AntennaArrayShape
C# 
public virtual AntennaArrayShape AntennaArrayShape {get; set;}
C++/CLI 
public:
virtual property AntennaArrayShape AntennaArrayShape {
   AntennaArrayShape get();
   void set (    AntennaArrayShape value);
}

Property Value

The default value is Linear.

Remarks

Allows the user to specify the antenna array shape.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 22.20

See Also