Keysight 89600 VSA .NET API
CyclicPrefixLengthMode Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : CyclicPrefixLengthMode Property


Glossary Item Box

Gets or sets the Cyclic Prefix length mode as being auto-detected, normal or extended.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property CyclicPrefixLengthMode As CyclicPrefixLengthModeType
C# 
public abstract CyclicPrefixLengthModeType CyclicPrefixLengthMode {get; set;}
C++/CLI 
public:
abstract property CyclicPrefixLengthModeType CyclicPrefixLengthMode {
   CyclicPrefixLengthModeType get();
   void set (    CyclicPrefixLengthModeType value);
}

Property Value

The default value is CyclicPrefixLengthModeType.Auto.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also