Gets or sets the highest frequency of the UL operating band.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property FrequencyHighUL As Double |
| C# | |
|---|
public abstract double FrequencyHighUL {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double FrequencyHighUL {
double get();
void set ( double value);
} |
Property Value
The default value is 1980 MHz (corresponding to E-UTRA Operating Band 1). The minimum value is
FrequencyLowUL and the maximum value is 5 GHz.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 15.00
See Also