| Visual Basic (Declaration) | |
|---|---|
Public Overloads Overridable Sub ImportLteSettings( _ ByVal fileName As String, _ ByVal testModel As Boolean _ ) | |
Parameters
- fileName
- The setup file to import LTE parameters from.
- testModel
- Indicates whether the setup file being imported is an E-TM setup. If this is an LTE-A carrier, setting this parameter to true causes the CellIdentity to be automatically incremented based on the component carrier index. If this is not an LTE-A carrier, the parameter has no effect.
Import of LTE parameters from setup files containing more than one measurement is not supported. This method can be used to import settings from an LTE setup file into an LTE-Advanced component carrier.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 20.00