Keysight 89600 VSA .NET API
ImportLteSettings Method
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : ImportLteSettings Method


Glossary Item Box

Import only LTE setup parameters from a setup file

Overload List

OverloadDescription
ImportLteSettings(String)Import only LTE setup parameters from a setup file  
ImportLteSettings(String,Boolean)Import only LTE setup parameters from a setup file  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also