Keysight 89600 VSA .NET API
InputChannel Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : InputChannel Property


Glossary Item Box

Gets or sets the reference measurement input channel.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property InputChannel As InputChannelType
C# 
public abstract InputChannelType InputChannel {get; set;}
C++/CLI 
public:
abstract property InputChannelType InputChannel {
   InputChannelType get();
   void set (    InputChannelType value);
}

Property Value

The default value is InputChannelType.Channel1.

Remarks

This value is ignored if the number if measurement input channels is 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also