Keysight 89600 VSA .NET API
IsCarrierIndicatorFieldPresent Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsCarrierIndicatorFieldPresent Property


Glossary Item Box

Gets or sets a value indicating whether the Carrier Indicator Field is present in the DCI messages.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsCarrierIndicatorFieldPresent As Boolean
C# 
public virtual bool IsCarrierIndicatorFieldPresent {get; set;}
C++/CLI 
public:
virtual property bool IsCarrierIndicatorFieldPresent {
   bool get();
   void set (    bool value);
}

Remarks

This property is meaningful only if the carrier is an LTE-A carrier. If IsCrossCarrierSchedulingEnabled is true, this property is forced to be true as well.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also