Keysight 89600 VSA .NET API
IsIncludeInactivePathsEnabled Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : IsIncludeInactivePathsEnabled Property


Glossary Item Box

Gets or sets a value indicating whether antenna paths below the antenna detection threshold (-36 dB default) in power from the reference antenna path are shown or blanked on the MIMO traces.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsIncludeInactivePathsEnabled As Boolean
C# 
public abstract bool IsIncludeInactivePathsEnabled {get; set;}
C++/CLI 
public:
abstract property bool IsIncludeInactivePathsEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also