| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property SchedulingCellId As Integer | |
| C# | |
|---|---|
public virtual int SchedulingCellId {get; set;} | |
This property is meaningful only if the carrier is an LTE-A carrier. If IsCrossCarrierSchedulingEnabled is false, this property is set to the same value as ServingCellIndex. Setting the property has no effect for the PCell, i.e. the cell with the ServingCellIndex of 0.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00