Keysight 89600 VSA .NET API
UplinkEMTCPuschAbsSubframeNumber Property
See Also 
Agilent.SA.Vsa.Lte.Interfaces Assembly > Agilent.SA.Vsa.Lte Namespace > MeasurementExtension Class : UplinkEMTCPuschAbsSubframeNumber Property


Glossary Item Box

Gets or sets the number of absolute subframes over which PUSCH repeats. this parameter needs to be set when the IsEMTCAnalysis is true

Syntax

Visual Basic (Declaration) 
Public Overridable Property UplinkEMTCPuschAbsSubframeNumber As Integer
C# 
public virtual int UplinkEMTCPuschAbsSubframeNumber {get; set;}
C++/CLI 
public:
virtual property int UplinkEMTCPuschAbsSubframeNumber {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.20

See Also