| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property CyclicShiftFieldFromDci As Integer | |
| C# | |
|---|---|
public abstract int CyclicShiftFieldFromDci {get; set;} | |
Property Value
The default value is 0. The minimum value is 0 and the maximum is 7.This parameter is used only when IsUsingCSFieldFromDci is set to true.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.0