Keysight 89600 VSA .NET API
NumberOfEutraCrsAntennas Property
See Also 
Agilent.SA.Vsa.NBIot.Interfaces Assembly > Agilent.SA.Vsa.NBIot Namespace > MeasurementExtension Class : NumberOfEutraCrsAntennas Property


Glossary Item Box

Gets or sets the number of CRS antenna ports that the LTE carrier uses.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property NumberOfEutraCrsAntennas As NumberOfEutraCrsAntennaPortsType
C# 
public abstract NumberOfEutraCrsAntennaPortsType NumberOfEutraCrsAntennas {get; set;}
C++/CLI 
public:
abstract property NumberOfEutraCrsAntennaPortsType NumberOfEutraCrsAntennas {
   NumberOfEutraCrsAntennaPortsType get();
   void set (    NumberOfEutraCrsAntennaPortsType value);
}

Property Value

The default value is NumberOfEutraCrsAntennaPortsType.One

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also