| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property ResultLength As Integer | |
| C# | |
|---|---|
public abstract int ResultLength {get; set;} | |
Property Value
The default value is 20 slots. The minimum value is 1 slot and the maximum is 100 slots.ResultLength, AnalysisStartBoundary, and IsNtmSignalAutoDetect determine the amount of data acquired.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)