Keysight 89600 VSA .NET API
FrequencyOffset Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > CarrierMapping Class : FrequencyOffset Property


Glossary Item Box

Gets or sets the frequency offset in hertz of this carrier mapping, relative to the Center value of Agilent.SA.Vsa.Measurement.Frequency.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property FrequencyOffset As Double
C# 
public abstract double FrequencyOffset {get; set;}
C++/CLI 
public:
abstract property double FrequencyOffset {
   double get();
   void set (    double value);
}

Property Value

The default value is 0 Hz.

Remarks

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also