Keysight 89600 VSA .NET API
SymbolPhaseCompensationFrequency Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > CarrierMapping Class : SymbolPhaseCompensationFrequency Property


Glossary Item Box

Gets or sets frequency used for symbol phase compensation of the signal under test.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SymbolPhaseCompensationFrequency As Double
C# 
public virtual double SymbolPhaseCompensationFrequency {get; set;}
C++/CLI 
public:
virtual property double SymbolPhaseCompensationFrequency {
   double get();
   void set (    double value);
}

Property Value

The default value comes from ComponentCarrier.SymbolPhaseCompensationManualFrequency.

Remarks

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also