| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property RadioFrameAllocationPeriod As MbsfnRadioFrameAllocationPeriod | |
| C# | |
|---|---|
public abstract MbsfnRadioFrameAllocationPeriod RadioFrameAllocationPeriod {get; set;} | |
| C++/CLI | |
|---|---|
public: abstract property MbsfnRadioFrameAllocationPeriod RadioFrameAllocationPeriod { MbsfnRadioFrameAllocationPeriod get(); void set ( MbsfnRadioFrameAllocationPeriod value); } | |
Property Value
Default value isRadio-frames that contain MBSFN subframes occur when equation SFN mod RadioFrameAllocationPeriod = is satisfied. Value denotes value 1, denotes value 2, and so on. When fourFrames is used for subframeAllocation, the equation above defines the first radio frame. Values and are not applicable when fourFrames is used. , ,
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00