Keysight 89600 VSA .NET API
ScramblingIdZero Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdsch Class : ScramblingIdZero Property


Glossary Item Box

Gets or sets a value indicating the scramblingID0 value used for DMRS sequence generation.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ScramblingIdZero As Integer
C# 
public virtual int ScramblingIdZero {get; set;}
C++/CLI 
public:
virtual property int ScramblingIdZero {
   int get();
   void set (    int value);
}

Property Value

Default value is 0. Range of value is 0 through 65535.

Remarks

This property corresponds to the higher-layer parameter scramblingID0 in DMRS-DownlinkConfig information element. Before VSA 25.20, NidNscid along with Nscid are used for DMRS sequence generation. According to 38211-g10 7.4.1.1.1, NidNscid is decided by Nscid, DmrsNidSource, ScramblingIdZero and ScramblingIdOne. From VSA 25.20 on, Nscid, DmrsNidSource, ScramblingIdZero and ScramblingIdOne are used for DMRS sequence generation. when Nscid is 0 and DmrsNidSource is DmrsNidSource.FromHigherLayer, ScramblingIdZero is used as NidNscid. when Nscid is 1 and DmrsNidSource is DmrsNidSource.FromHigherLayer, ScramblingIdOne is used as NidNscid.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.20

See Also