| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property IsDmrsSequenceValid As Boolean | |
| C# | |
|---|---|
public virtual bool IsDmrsSequenceValid {get; set;} | |
Property Value
The default value is true.When true, the DMRS can be used for initial synchronization SynchronizationSource, phase/timing/amplitude tracking based on TrackingSignalBasis, and also can be used for channel estimation based on EqualizerTrainingSignalBasis. When equalization is on, the data on this PUSCH will be equalized with the channel estimation based on this DMRS sequence. When false, the data on this PUSCH will not be equalized.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00