| Visual Basic (Declaration) | |
|---|---|
Public Property AreDemodPropertiesOverridden As Boolean | |
| C# | |
|---|---|
public bool AreDemodPropertiesOverridden {get; set;} | |
When this value is true, ResultLengthInSubframe, FrameTriggerEnabled and DecodeMaxIteration are set by the values in this CalculationControl. When this value is false, all these demodulation properties are set by the VSA setx file when calling NewRadioDirectCalculation.ConfigureWithVsaSetupFile.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)