| Visual Basic (Declaration) | |
|---|---|
Public Property TimeDomainSignalCarrierCenterFrequency As Double | |
| C# | |
|---|---|
public double TimeDomainSignalCarrierCenterFrequency {get; set;} | |
When InputDataDomain is InputDataDomain.Time, and AreDemodPropertiesOverridden is true, this value indicates the component carrier center frequency in Hz within the time domain input signal. If value is set to double.NaN it will not be applied (so ignored).
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00