| Visual Basic (Declaration) | |
|---|---|
Public Property TimeDomainSignalSampleRate As Double | |
| C# | |
|---|---|
public double TimeDomainSignalSampleRate {get; set;} | |
When InputDataDomain is InputDataDomain.Time, and AreDemodPropertiesOverridden is true, this value indicates the sampling rate in Hz of the time domain input signal. Only sampling rate values > 0 will be applied (otherwise the value is ignored).
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.40