| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Sub ConfigureNoncontiguousCarriers( _ ByVal numberOfCarriers As Integer, _ ByVal carrierSpacing As Double, _ ByVal carrierIndexBeforeNoncontiguousBreak As Integer _ ) | |
| C# | |
|---|---|
public abstract void ConfigureNoncontiguousCarriers( int numberOfCarriers, double carrierSpacing, int carrierIndexBeforeNoncontiguousBreak ) | |
| C++/CLI | |
|---|---|
public: abstract void ConfigureNoncontiguousCarriers( int numberOfCarriers, double carrierSpacing, int carrierIndexBeforeNoncontiguousBreak ) | |
Parameters
- numberOfCarriers
- The number of carriers to configure.
- carrierSpacing
- The spacing between carrier centers in Hz.
- carrierIndexBeforeNoncontiguousBreak
- The index of the carrier after which a new subblock begins.
This function will keep the existing CarrierConfigurations intact while adjusting some of their configuration values and will fill in the missing CarrierConfigurations to match the numberOfCarriers. Call this function also sets the ChannelRaster to ChannelRaster.None and the ChannelSpacing to ChannelSpacing.AdjacentCarriers.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)