Keysight 89600 VSA .NET API
AntennaOrientation Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > AngleOfArrival Class : AntennaOrientation Property


Glossary Item Box

Gets or sets a value indicating the antenna orientation to use.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AntennaOrientation As AoaAntennaOrientation
C# 
public abstract AoaAntennaOrientation AntennaOrientation {get; set;}
C++/CLI 
public:
abstract property AoaAntennaOrientation AntennaOrientation {
   AoaAntennaOrientation get();
   void set (    AoaAntennaOrientation value);
}

Property Value

The default value is AoaAntennaOrientation.Disabled.

Remarks

Changing the AntennaOrientation configures the Antennas by enabling and positioning the AoaAntennas based upon the AoaAntennaOrientation and the AntennaSpacing.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also