Gets or sets the time offset for pulse-to-pulse analysis, relative to the reference.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property PulseToPulseAnalysisOffset As Double |
| C# | |
|---|
public abstract double PulseToPulseAnalysisOffset {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double PulseToPulseAnalysisOffset {
double get();
void set ( double value);
} |
Property Value
The unit seconds. The default value is 0 seconds.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 19.00
See Also