Keysight 89600 VSA .NET API
PulseToPulseAnalysisReference Property
See Also 
Agilent.SA.Vsa.Pulse.Interfaces Assembly > Agilent.SA.Vsa.Pulse Namespace > MeasurementExtension Class : PulseToPulseAnalysisReference Property


Glossary Item Box

Gets or sets the reference time for specifying pulse-to-pulse analysis part.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PulseToPulseAnalysisReference As PulseToPulseAnalysisReference
C# 
public abstract PulseToPulseAnalysisReference PulseToPulseAnalysisReference {get; set;}
C++/CLI 
public:
abstract property PulseToPulseAnalysisReference PulseToPulseAnalysisReference {
   PulseToPulseAnalysisReference get();
   void set (    PulseToPulseAnalysisReference value);
}

Property Value

The default value is Center.

Remarks

This property is used only if IsPulseToPulseSameAsFrequencyPhaseAnalysisPart is false. The actual pulse-to-pulse analysis part, relative to this reference, is determined by PulseToPulseAnalysisOffset and PulseToPulseAnalysisWindowLength.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00

See Also