Keysight 89600 VSA .NET API
OffsetSide Property
See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace > Offset Class : OffsetSide Property


Glossary Item Box

Gets or sets which side of offsets are enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property OffsetSide As OffsetSide
C# 
public abstract OffsetSide OffsetSide {get; set;}
C++/CLI 
public:
abstract property OffsetSide OffsetSide {
   OffsetSide get();
   void set (    OffsetSide value);
}

Property Value

The default value is OffsetSide.Both.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also