Keysight 89600 VSA .NET API
Offset Class Members
See Also  Properties  Methods  Events
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace : Offset Class

Glossary Item Box

The following tables list the members exposed by Offset.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyEnabledGets or sets a value indicating whether to measure this Offset.  —
Public PropertyIntegrationBandwidthGets or sets the equivalent noise bandwidth (in Hz) used when calculating power in the offset.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsInnerGets or sets a value indicating whether this offset is an inner offset or not.  —
Public PropertyLimitGets a reference to a PowerLimit object, which defines the limits associated with this offset definition.  —
Public PropertyLowerSpectrumChannelIndexGets or sets a value indicating (by index) which item in Channels to use for this Offset for Lower region.  27.00
Public PropertyOffsetSideGets or sets which side of offsets are enabled.  —
Public PropertyReferenceSubblock1Gets or sets the ID of subblock1 this offset is referencing.  —
Public PropertyReferenceSubblock2Gets or sets the ID of subblock2 this offset is referencing.  —
Public PropertyReferenceSubblock2EnabledGets or sets a value indicating whether the ReferenceSubblock2 is used as a reference or not.  —
Public PropertyRelativeFrequencyGets or sets the offset frequency (in Hz) as an offset from the carrier reference frequency  —
Public PropertyRrcFilterAlphaGets or sets the roll off factor of the RRC filter used if RrcFilterEnabled is set to true.  —
Public PropertyRrcFilterEnabledGets or sets a value indicating whether carrier power calculations are weighted with a root-raised-cosine filter.  —
Public PropertyUpperSpectrumChannelIndexGets or sets a value indicating (by index) which item in Channels to use for this Offset for Upper region.  27.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also