Keysight 89600 VSA .NET API
RrcFilterAlpha Property
See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace > Offset Class : RrcFilterAlpha Property


Glossary Item Box

Gets or sets the roll off factor of the RRC filter used if RrcFilterEnabled is set to true.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property RrcFilterAlpha As Double
C# 
public abstract double RrcFilterAlpha {get; set;}
C++/CLI 
public:
abstract property double RrcFilterAlpha {
   double get();
   void set (    double value);
}

Property Value

The default value is 0.22.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also