Keysight 89600 VSA .NET API
RrcFilterEnabled Property
See Also 
Keysight.SA.Vsa.AdjacentChannelPower.Interfaces Assembly > Keysight.SA.Vsa.AdjacentChannelPower Namespace > Offset Class : RrcFilterEnabled Property


Glossary Item Box

Gets or sets a value indicating whether carrier power calculations are weighted with a root-raised-cosine filter.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property RrcFilterEnabled As Boolean
C# 
public abstract bool RrcFilterEnabled {get; set;}
C++/CLI 
public:
abstract property bool RrcFilterEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also