| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property CrossCorrelatedEvmEnabled As Boolean | |
| C# | |
|---|---|
public virtual bool CrossCorrelatedEvmEnabled {get; set;} | |
Currently only supports two channels. Both channels must capture the same exact data.
- Configure Pattern Search and then set CrossCorrelatedEvmEnabled to true to enable cross-correlated EVM
- Use CarrierAggregation.ConfigureCrossCorrelatedEvm to set up cross-correlated EVM
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.40