The following tables list the members exposed by MeasurementExtension.
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | CarrierAggregation | Gets a reference to the CarrierAggregation settings where carriers can be defined and configured. | — |
![]() | ConfigurationMode | Gets or sets the programming mode of the FlexFrame API. | 30.00 |
![]() | CrossCorrelatedEvmEnabled | Gets or sets a value indicating whether to compute cross-correlated EVM between two measurement channels. | 27.40 |
![]() | CustomModulations | Gets the user-defined collection of imported custom modulations CustomModulationCollection. | 27.40 |
![]() | IsDisposed | Gets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | IsEvmReportedInDecibels | Gets or sets a value indicating whether to show EVM metrics on summary traces in units of dB instead of units of percent (%). | — |
![]() | OutputPointsPerSymbol | Gets or sets the number of points per symbol displayed in traces (IQ Meas, IQ Ref, Error Vector, etc.). | — |
![]() | QuickSetups | Gets a reference to the collection of available factory-provided and user-defined QuickSetup objects which may be used to configure FlexFrame analysis. | 26.00 |
![]() | ResultLength | Gets or sets the number of symbols to provide in the results of the measurement. | — |
![]() | SearchLength | Gets or sets the search interval (for finding the ResultLength) in seconds when Style = FrameDefinitionStyle.Burst. | — |
![]() | SingleCarrier | Gets a reference to the SingleCarrier | 30.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() ![]() | CastToExtensionType | This method casts the supplied object to the MeasurementExtension type. Some tools are unable to use the generic methods provided on Agilent.SA.Vsa.Measurement class so this is provided as an alternative. | — |
![]() | ConfigureCrossCorrelatedEvm | Obsolete. For ConfigurationMode = ConfigurationModeSelection.Advanced, use CarrierAggregation.ConfigureCrossCorrelatedEvm instead. Otherwise, see CrossCorrelatedEvmEnabled. | 27.40 |
![]() | CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject) | — |
![]() ![]() | ExtensionType | Returns the type for instances this measurement extension. Some tools are unable to use the generic methods provided on Agilent.SA.Vsa.Measurement class so this is provided as an alternative. | — |
![]() | ForceRebuildKeyMap | This method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject) | — |
![]() | InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | Preset | Preset the FlexFrame measurement. | — |
![]() | SaveWaveformToFile | Saves the generated waveform to a file for one carrier or for all carriers, writing in MAT v7 format via the platform data-file utility. | 30.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | PropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | PropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | 14.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||