Measurement Interval (802.16 OFDM)
: See 802.16 OFDM Standard Setups/Presets Table.
specifies the time length of Result Length data that is used for computing and displaying the trace data results. is entered as an integer number of Symbol-times. See Measurement Interval and Offset for more information about this parameter and its application.
The value must be less than or equal to the Result Length or Maximum Result Length parameter (depending on which option is selected for Result Length). This parameter combined with specifies the portion of the Result Length to analyze and display to the user.
See Also
Result Length Parameters (802.16 OFDM)
Measurement Offset (802.16 OFDM)