Inst Spectrum (802.16 OFDM)
(Instantaneous Spectrum) shows the frequency spectrum of the pre-demodulated time data. The time data is windowed and FFTed to create the display.
If is ON, trace data is the results of the . If averaging is on, the does not show the effects of averaging. To see the effects of averaging, use the trace data. If averaging is not on, this is identical to the data (refer to the Digital Demodulation Block Diagram.
See Also