Time (802.16 OFDM)
When Demodulation is enabled, the trace shows the time record before digital demodulation and after pulse search, as shown in the following block diagram (refer to the Digital Demodulation Block Diagram).

The amount of data included in the trace trace data is a function of the , and Measurement Offset parameters. The following topics describe how these parameters affect the Time trace data:
-
trace data and Result Length Parameters
-
trace data and Measurement Interval and Offset parameters
-
trace data and Averaging
Time trace data and Result Length parameters
-
Automatic / From FCH modes: The trace data shows the data specified by the Max Result Length parameter:
-
If is less than the burst length, the trace data shows the number of symbol-times specified by the parameter +/- 10% of the plus the preamble.
-
If is greater than the burst length, the trace data shows the entire burst +/- 10% of the burst length (includes the preamble).

For more information about how the parameter determines the measurement result length, see Result Length Parameters.
-
-
Manual mode: The trace data shows data for the number of symbol-times specified by the parameter plus 10% of the length plus the preamble.
For more information about how the parameter determines the measurement result length data, see Result Length Parameters.
Time trace data and Measurement Interval/Offset parameters
-
not equal to
When the and parameters are used to specify the acquired measurement data, the trace data includes only the data specified by the parameter. The trace data shows only data for the symbol-times specified within the all other data before and after the is excluded. This also means that preamble data will not be shown when using and parameters.
-
equal to
When the is equal to , the trace data is controlled and specified by the parameter, see Automatic mode described previously for more information.
For more information about how and determine the measurement result length data, refer to Measurement Interval and Offset.
Time trace data and Averaging
trace data is unaffected by time averaging.
See Also