Measure Input Channel (802.16 OFDMA)
:Channel 1 (See OFDMA Standard Presets Table.)
selects one of the input channels as the source for the STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively./MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. measurements.
How the parameter affects the VSA depends on the status of the Enable Matrix Decoder parameter.
- When the parameter is cleared, the parameter selects one of the input channels for regular OFDMA analysis. For example, if Antenna 0 is selected, then the Antenna 0 pilot pattern is used for OFDMA analysis for the selected input channel.
- When the parameter is selected, the parameter (along with the Override Transmit Antenna Pilot Pattern parameter) selects which Tx/Rx path to isolate from the MIMO traces into legacy traces for better visibility. These legacy traces include , , , and .
The STC/MIMO measurement results can be viewed in the MIMO
Info trace.
See Also