Measure Matrix Stream (802.16 OFDMA)
: Stream 1 (See OFDMA Standard Presets Table.)
selects the matrix stream for analysis.
is only available when the Enable
Matrix Decoder checkbox is selected.
The matrix analyzed by the Matrix Decoder (A or B) is selected on the using the STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively. Matrix parameter on the Zone Definition Panel.
See Also