Map File Editor Dialog Box (802.16 OFDMA)
The dialog box provides the interface to create and edit the map file uplink and downlink subframe zone definitions.
The features of the dialog box are:
- : used to display and edit the name of the current map file.
- Downlink/Uplink Zones list box: lists the existing downlink/uplink zone definitions for the specified map file.
- : opens the Edit Zone Definition section to create a new downlink/uplink zone definition. When is clicked the Zone Definition Editor for Map Files is opened.
- : opens the Edit Zone Definition section to edit the selected downlink/uplink zone definition. When Edit is clicked and a Zone is selected, the Zone Definition Editor for Map Files is opened.
- : deletes the selected downlink/uplink zone.
- : copies an existing zone definition to the current map file from either a Definition Source or an existing Map File.
- : selects whether the Map File is shared between all users or is private to the currant user.
- checkbox
- Zone Definition
- Bursts in Selected Zone
-
- checkbox
See Also