Analysis Offset (802.16 OFDMA)
: 0 Frames (See OFDMA Standard Presets Table.)
specifies the number of frames that are offset from the start of the data acquisition. is used to specify what frame is used for analysis within the measurement .
See Also
: 0 Frames (See OFDMA Standard Presets Table.)
specifies the number of frames that are offset from the start of the data acquisition. is used to specify what frame is used for analysis within the measurement .
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |