Acquisition Length (802.16 OFDMA)
: 1 frames (See OFDMA Standard Presets Table.)
determines the signal capture length in terms of contiguous OFDMA frames. This is the data used by the VSA for demodulation and signal analysis.
Make sure that the is long enough to capture all the desired data.
The determines the maximum input time record that can be shown on the Search Time and Raw Main Time trace data outputs.
See Also