Include Transition Regions (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
adds an additional 10% of time domain data before and after the specified in the time trace. For the selection of , the extra time data is added to the end of the data region
is useful for observing signal transitions before and after the analysis region.
See Also