Measurement Region (non-demod) (802.16 OFDMA)
: Demodulation (See OFDMA Standard Presets Table.)
When Manual is selected for the Definition Source, the parameter selects a pre-defined region of the time record to include in the trace and therefore also defines what time domain data is used to compute the trace and traces.
The selections are:
- Frame: includes the Frame region (preamble+DLSubframe+ULSubframe)
- Zone: includes the entire zone that is active for analysis
- Demodulation: includes the portion of the waveform used by the demodulator
- Preamble: includes the Preamble
Also included in the Measurement Region are:
See Also