Measurement Interval (802.16 OFDMA)
: 1 Symbols (See OFDMA Standard Presets Table.)
When is selected, in conjunction with manually specifies a "zoomed" measurement analysis region (in time) to a specific segment of the defined zone or set of defined data bursts without re-defining the input signal. The measurement is restricted to the defined signal.
See Also